The Latest in Releasing Control Panel Technology
Viking's VFR-500 Conventional Multi-Hazard Releasing Panel has been designed to expand upon the previous generation's strengths while enhancing an already robust feature set. With focus directed toward simplifying the installation process and a greater emphasis on control of monitoring and maintenance, the VFR-500 is equipped for your fire protection needs.
Expanded Feature Set
Intuitive User Interface
The VSF-500 Releasing Panel has been revamped to provide an intuitive user interface. Some of these upgrades include a 30% larger display, additional navigation buttons, an expanded history that holds up to 4,000 events, keypad programmability and the ability to program using a computer.

User Definable Zones
Viking's VSF-500 Releasing Panel features seven zones that are user definable. This is an increase of three additional user definable zones that grant greater user customization from the previous generation.

Multidirectional Navigation
The VSF-500 allows for multidirectional navigation through the panel history and menus, allowing for a more intuitive and user-friendly experience than its predecessor.

Built-in Notification Appliance Patterns and Synchronization
Notification appliances' strobe synchronization is now built into the panel, no longer requiring separate modules for synchronization. The strobe synchronization includes Gentex, AMSECO, System Sensor and Cooper/Wheelock protocols with Quadrasync technology, each output circuit can have a unique manufacturer of strobes, meaning you can mix and match while having all of the strobes flash together. With built-in notification patterns, it allows for the use of the same notification appliance to annunciate different parts of the releasing sequence uniquely, allowing the evacuation signal, prerelease signal and release signal all to be on one circuit.
Increased Power Resources
The VSF-500 has increased the total panel output from a maximum output of 2.5 A to 3.0 A. The output circuits can use the full power of the panel with a maximum output of 3.0 A per output which is increased from the previous 1.0 A.
Ease of Installation
Hassle Free Installation
Viking's VSF-500 was designed for an effortless transition from installations using the previous model. The VSF-500's housing retains all the same wiring terminations and footprint allowing for the layout to be preserved, all while utilizing the same common conduit locations.
Full Deadfront with Hook System
The VSF-500 features a full deadfront which creates added safety when the cabinet is open for interfacing while in service. The deadfront is designed with a hook system that allows it to be hung from the enclosure during installation and servicing.
Optional Disable Switch
Mounted inside the VSF-500 enclosure, the optional RCDS-PM releasing circuit disable switch allows for disabling one or two releasing zones.
Monitoring and Maintenance
Remote Management via Email
The VFR-500 allows for users to remotely retrieve data from the releasing panel when necessary. Users can receive monitoring updates through e-mail including critical reminders for testing, event buffer, and panel conditions like troubles and alarms.* This gives control over how monitoring and maintenance are managed.
*Non-UL Listed Feature
Flexible Programming
User definable programming of the VFR-500 can be completed at the panel using its built-in menus or from the Panel Programmer software.
Optional Disable Switch
The VFR-500 has a proprietary P-Link protocol allowing the addition of up to thirty-one accessories including remote annunciators, an intelligent power supply, additional input cards and more!
Check out these additional resources
Review the available resources to make sure you know everything there is to know about the VFR-500 Releasing Control Panel.